Topology
- Slave devices can have several ports.
- Using these features, EtherCAT can support almost any physical topology (e.g., line, tree, or star).
- The bus or line structure known from the fieldbuses An industrial network system for real-time distributed control (e.g., CAN or PROFIBUS, Sercos®). It is a way of connecting instruments in a plant design. is then available for Ethernet.
The combination of line and branches or stubs is also possible.
- Any EtherCAT device with three or more ports can act as a junction; no additional switches are required.
- The classic switch-based Ethernet star topology can be used either with switches configured to forward traffic directly The orientation components of a vector in space. between ports, or with special slave devices.
- The switches are then located between the network master and the slave devices.
The special slave device assembly (i.e., standard slave devices don't have a MAC address A Media Access Control (MAC) address is a quasi-unique identifier assigned to most network adapters or network interface cards (NICs) by the manufacturer for identification. If assigned by the manufacturer, a MAC address usually encodes the manufacturer's registered identification number.) attached to one switch port together forms an EtherCATsegment. This is either addressed via its MAC address or via port-based VLANs.
- Since the 100BASE-TX Ethernet physical layer is used, the distance between any two nodes can be up to a maximum of 100 m (300 ft).
- Up to 65535 devices can be connected per segment.
- If an EtherCAT network is wired in ring configuration (requiring two ports on the master device), it can provide cable redundancy.
Figure 1: Flexible Topology: Line, Tree, or Star
- KAS Kollmorgen Automation Suite controllers support line, tree, and star topologies.
- Ring topologies and cable redundancy is not supported because the KAS controllers have a singe EtherCAT port.